2023-02-22 5:07 AM
Regarding P/N: STM32WB55 in a WLCSP100 package:
Q1: When VBAT is not in use, can I connect it to GND?
Q2: When VDDA is not in use, it must be connected to VDD, but is it still requires a 10 nF + 1 μF capacitors?
Q3: If VDDA is not in use, can I connect VREF+ to GND?
Thanks!
Nir
Solved! Go to Solution.
2023-03-01 4:14 AM
Q1: VBAT to VDD
Q2: Not necessary the 10nF + 1uF
Q3: Yes, customer can connect to GND
2023-03-01 4:14 AM
Q1: VBAT to VDD
Q2: Not necessary the 10nF + 1uF
Q3: Yes, customer can connect to GND
2023-03-02 1:11 AM
Thanks a lot!