2024-06-19 12:55 AM
Hello, I have a question about the internal antenna of the STM32WB55CGU6.
First of all, does it have the internal antenna? And if so, what is the range of it?
Thanks
Solved! Go to Solution.
2024-06-19 02:04 AM
Hello @Bond00914 and welcome to the ST Community 😊.
the STM32WB55CGU6 is an MCU and does not include an internal antenna. But if you are toking about the evaluation board P-NUCLEO-WB55 that use the STM32WB55CGU6, it includes a PCB Antenna that is used as the default antenna. And a SMA Antenna that need to Connect a 50ohms Instrument or antenna so that we can use it:
For the range, it depends on different external characteristics (TX Power, ...). But we can estimate about Few meters (maybe up to 20m).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-19 02:04 AM
Hello @Bond00914 and welcome to the ST Community 😊.
the STM32WB55CGU6 is an MCU and does not include an internal antenna. But if you are toking about the evaluation board P-NUCLEO-WB55 that use the STM32WB55CGU6, it includes a PCB Antenna that is used as the default antenna. And a SMA Antenna that need to Connect a 50ohms Instrument or antenna so that we can use it:
For the range, it depends on different external characteristics (TX Power, ...). But we can estimate about Few meters (maybe up to 20m).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.