2022-08-03 02:17 AM
Hi, I have shared my project schematic. it's should work or not? (SMPs not used)
Problem : BLE cannot advertise, but this configuration in STM32CubeIDE can work with NUCLEO-WB55.
Solved! Go to Solution.
2022-08-09 04:49 AM
Hello.
Now my custom board is working.
This is my solution step by step and some problem I saw in code generation.
STM32CudeIDE version 1.10.1
STM32WBCube version 1.14.1
#1 : Install wireless stack firmware. (new IC MCU)
For new IC MCU need to flash wireless stack firmware. In my case user stm32wb1x_BLE_Stack_full_fw.bin found in
../../STM32Cube/Repository/STM32Cube_FW_WB_V1.14.1/Projects/STM32WB_Copro_Wireless_Binaries/STM32WB1x/stm32wb1x_BLE_Stack_full_fw.bin
upload this firmware to the MCU by using STM32CubeProgrammer start address 0x08021000
please see instructions in "Release_Notes.html" (important)
#2 : Test with example
This step make sure your board can work.
In my case I test with BLE_HeartRate example.
../../STM32Cube/Repository/STM32Cube_FW_WB_V1.14.1/Projects/NUCLEO-WB15CC/Applications/BLE/BLE_HeartRate
Import to STM32CudeIDE and compile without change anything the start debug or just upload to the board
#3 : Create new project
Please follow project configuration in YouTube STMicroelectronics channel
Simple BLE application generated from CubeMX
for STM32WB15xx please change some configuration because of RAM limitation ref: NUCLEO-STM32WB15 HardFault Error with BLE custom Template.
config : (in example use this config value I don't known how to calculation )
Minimum Heap Size : 0x400
Minimum Stack Size : 0x1000
# 3.1 Fix code generation (for 1.14.1)
# fix startup script (this bug or developer need to change manually? )
replace all script startup_stm32wb15ccux.s generated with STM32CudeIDE by startup_stm32wb15ccux.s script in BLE_HeartRate example project. (see #2)
# fix app_entry.c
In this step the BLE can advertise but not normal working (don't known why). GPIO repeat toggle without init or not using (my LED blink repeatedly). I have fixed by modified in MX_APPE_Init() function code generated with
void MX_APPE_Init(void)
{
System_Init(); /**< System initialization */
SystemPower_Config(); /**< Configure the system Power Mode */
HW_TS_Init(hw_ts_InitMode_Full, &hrtc); /**< Initialize the TimerServer */
/* USER CODE BEGIN APPE_Init_1 */
APPD_Init();
/**
* The Standby mode should not be entered before the initialization is over
* The default state of the Low Power Manager is to allow the Standby Mode so an request is needed here
*/
UTIL_LPM_SetOffMode(1 << CFG_LPM_APP, UTIL_LPM_DISABLE);
/* USER CODE END APPE_Init_1 */
appe_Tl_Init(); /* Initialize all transport layers */
/**
* From now, the application is waiting for the ready event (VS_HCI_C2_Ready)
* received on the system channel before starting the Stack
* This system event is received with APPE_SysUserEvtRx()
*/
/* USER CODE BEGIN APPE_Init_2 */
/* USER CODE END APPE_Init_2 */
return;
}
# Compile and Run ➡�?
# Found some bug (or I missed something?)
In code generation I can't start advertising with low power mode by change APP_BLE_FAST_ADV to APP_BLE_LP_ADV in Adv_Request(APP_BLE_LP_ADV); function.
because in this function always with fast mode ?
solution
BleApplicationContext.Device_Connection_Status = NewStatus;
/* Start Fast or Low Power Advertising */
ret = aci_gap_set_discoverable(ADV_TYPE,
NewStatus == APP_BLE_FAST_ADV ? CFG_FAST_CONN_ADV_INTERVAL_MIN : CFG_LP_CONN_ADV_INTERVAL_MIN,
NewStatus == APP_BLE_FAST_ADV ? CFG_FAST_CONN_ADV_INTERVAL_MAX : CFG_LP_CONN_ADV_INTERVAL_MAX,
CFG_BLE_ADDRESS_TYPE,
ADV_FILTER,
0,
0,
0,
0,
0,
0);
Thanks,
Chatchai
2022-08-09 04:49 AM
Hello.
Now my custom board is working.
This is my solution step by step and some problem I saw in code generation.
STM32CudeIDE version 1.10.1
STM32WBCube version 1.14.1
#1 : Install wireless stack firmware. (new IC MCU)
For new IC MCU need to flash wireless stack firmware. In my case user stm32wb1x_BLE_Stack_full_fw.bin found in
../../STM32Cube/Repository/STM32Cube_FW_WB_V1.14.1/Projects/STM32WB_Copro_Wireless_Binaries/STM32WB1x/stm32wb1x_BLE_Stack_full_fw.bin
upload this firmware to the MCU by using STM32CubeProgrammer start address 0x08021000
please see instructions in "Release_Notes.html" (important)
#2 : Test with example
This step make sure your board can work.
In my case I test with BLE_HeartRate example.
../../STM32Cube/Repository/STM32Cube_FW_WB_V1.14.1/Projects/NUCLEO-WB15CC/Applications/BLE/BLE_HeartRate
Import to STM32CudeIDE and compile without change anything the start debug or just upload to the board
#3 : Create new project
Please follow project configuration in YouTube STMicroelectronics channel
Simple BLE application generated from CubeMX
for STM32WB15xx please change some configuration because of RAM limitation ref: NUCLEO-STM32WB15 HardFault Error with BLE custom Template.
config : (in example use this config value I don't known how to calculation )
Minimum Heap Size : 0x400
Minimum Stack Size : 0x1000
# 3.1 Fix code generation (for 1.14.1)
# fix startup script (this bug or developer need to change manually? )
replace all script startup_stm32wb15ccux.s generated with STM32CudeIDE by startup_stm32wb15ccux.s script in BLE_HeartRate example project. (see #2)
# fix app_entry.c
In this step the BLE can advertise but not normal working (don't known why). GPIO repeat toggle without init or not using (my LED blink repeatedly). I have fixed by modified in MX_APPE_Init() function code generated with
void MX_APPE_Init(void)
{
System_Init(); /**< System initialization */
SystemPower_Config(); /**< Configure the system Power Mode */
HW_TS_Init(hw_ts_InitMode_Full, &hrtc); /**< Initialize the TimerServer */
/* USER CODE BEGIN APPE_Init_1 */
APPD_Init();
/**
* The Standby mode should not be entered before the initialization is over
* The default state of the Low Power Manager is to allow the Standby Mode so an request is needed here
*/
UTIL_LPM_SetOffMode(1 << CFG_LPM_APP, UTIL_LPM_DISABLE);
/* USER CODE END APPE_Init_1 */
appe_Tl_Init(); /* Initialize all transport layers */
/**
* From now, the application is waiting for the ready event (VS_HCI_C2_Ready)
* received on the system channel before starting the Stack
* This system event is received with APPE_SysUserEvtRx()
*/
/* USER CODE BEGIN APPE_Init_2 */
/* USER CODE END APPE_Init_2 */
return;
}
# Compile and Run ➡�?
# Found some bug (or I missed something?)
In code generation I can't start advertising with low power mode by change APP_BLE_FAST_ADV to APP_BLE_LP_ADV in Adv_Request(APP_BLE_LP_ADV); function.
because in this function always with fast mode ?
solution
BleApplicationContext.Device_Connection_Status = NewStatus;
/* Start Fast or Low Power Advertising */
ret = aci_gap_set_discoverable(ADV_TYPE,
NewStatus == APP_BLE_FAST_ADV ? CFG_FAST_CONN_ADV_INTERVAL_MIN : CFG_LP_CONN_ADV_INTERVAL_MIN,
NewStatus == APP_BLE_FAST_ADV ? CFG_FAST_CONN_ADV_INTERVAL_MAX : CFG_LP_CONN_ADV_INTERVAL_MAX,
CFG_BLE_ADDRESS_TYPE,
ADV_FILTER,
0,
0,
0,
0,
0,
0);
Thanks,
Chatchai