cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB09 MESH

TTIN.1562
Associate II

How to port BLE Mesh Lighting application SW for BNRGLP into STM32WB09?

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @TTIN.1562 

Currently there is only the STSW-BNRGLP-Mesh which is compatible with BlueNRG-LP (future STM32WB07), so it will not run properly on STM32WB09. Regarding mesh library support within STM32WB0 series and related SW framework, currently there is no plan and timeline for that.

Best Regards

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
STTwo-32
ST Employee

Hello @TTIN.1562 

I suggest you take a look at the AN6141. It should be really helpful.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello@ STTwo-32

Thanks for the suggestion.

AN6141 provides the steps need to do for porting BLEStack v3.x to 4.x.

However, target application needs BLE Mesh.

In v3.x, Mesh was supported as compiled LIB file.

For v4.x, is there any Mesh LIB supported?

Or how to port Mesh LIB from BULENRG to STM32B0?

Thanks and Best regards.

Hello @TTIN.1562 

Currently there is only the STSW-BNRGLP-Mesh which is compatible with BlueNRG-LP (future STM32WB07), so it will not run properly on STM32WB09. Regarding mesh library support within STM32WB0 series and related SW framework, currently there is no plan and timeline for that.

Best Regards

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.