cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 WPAN Remove BLE Service

dsmail1
Associate

Hello,

 

I have an existing STM32_WPAN configuration with 3 BLE services and I want to completely remove Service 2. Is there any way to do that?

 

dsmail1_1-1738857718804.png

 

I've already reduced the number of services to 2, but it ends up removing Service 3 which I want to keep. Is it possible to swap Service 2 and 3 and then reduce to 2 services.

dsmail1_2-1738857748359.png

 

thank you in advance

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @dsmail1 

For now, it is not possible to do this throw CubeMX. The only solution is to do it directly on the generated code. You can also create a new project and copy exactly the same configuration and code but only for two services. I’ve escalated a request to review the possibilty of implementing this on CubeMX directly (under internal ticket number 202528).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @dsmail1 

For now, it is not possible to do this throw CubeMX. The only solution is to do it directly on the generated code. You can also create a new project and copy exactly the same configuration and code but only for two services. I’ve escalated a request to review the possibilty of implementing this on CubeMX directly (under internal ticket number 202528).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.