cancel
Showing results for 
Search instead for 
Did you mean: 

Single bonded device in STM32WB

thealbertdev
Associate III

I am programming an STM32WB5MMG module. Is it possible to limit the number of bounded devices to one?

One process could be to bound to one device and when I want to bound another, delete all previously bounded devices. However, I would like to only delete the stored device once a new one has been successfully bounded. Is this possible?

My idea is to make use of the whitelist to only allow connections from the bounded device. The system has a button from which to deactivate the whitelist and allow a different device to be bounded (but as I said, I would like to only delete the old device if a new one is successfully bounded).

Best regards and thank you for your time.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
STTwo-32
ST Employee

Hello @thealbertdev 

I think your implementation can do the job. But you should first understand how works the bounding procedure.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.