cancel
Showing results for 
Search instead for 
Did you mean: 

Secure Flash Area Modification on STM32WB15CC ?

hanyang
Associate II

I am using the STM32WB15CC and encountered an issue when my program exceeded 112KB (0x1C000), causing the flashing process to fail. I noticed that the memory region starting from 0x0801C000 is set as a secure flash area.

I would like to know if it is possible to modify this secure flash area. If so, could you please provide guidance on how to make the necessary modifications?

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @hanyang 

To optimize the available memory for a dedicated application, the linker file must be updated. But the end of available Flash memory address can be moved only up to the SFSA address.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @hanyang 

To optimize the available memory for a dedicated application, the linker file must be updated. But the end of available Flash memory address can be moved only up to the SFSA address.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.