‎2021-08-29 3:05 AM
Hello, I am new to the STM32 world.
my little board STM32 (LoRa) form China
ST-LINK SN : 53FF6D066687505145250967
ST-LINK FW : V2J38S7
Board : --
Voltage : 3.26V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x699
Revision ID : Rev Z
Device name : STM32WLxx
Flash size : 128 KBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : 0xc2
Read Out Protection:
RDP : 0xAA (Level 0, no protection)
BOR Level:
BOR_LEV : 0x0 (BOR Level 0 reset level threshold is around 1.7 V)
User Configuration:
nBOOT0 : 0x1 (nBOOT0=1)
nBOOT1 : 0x1 ()
nSWBOOT0 : 0x1 (BOOT0 taken from PH3/BOOT0 pin)
SRAM_RST : 0x1 (SRAM1 and SRAM2 are not erased when a system reset occurs)
SRAM2_PE : 0x1 (SRAM2 parity check disable)
nRST_STOP : 0x1 (No reset generated when entering the Stop mode)
nRST_STDBY : 0x1 (No reset generated when entering the Standby mode)
nRST_SHDW : 0x1 (No reset generated when entering the Shutdown mode)
WWDG_SW : 0x1 (Software window watchdog)
IWGD_STDBY : 0x1 (Independent watchdog counter running in Standby mode)
IWDG_STOP : 0x1 (Independent watchdog counter running in Stop mode)
IWDG_SW : 0x1 (Software independent watchdog)
BOOT_LOCK : 0x0 (CPU1 CM4 Boot lock disabled)
C2BOOT_LOCK : 0x0 (CPU2 CM0+ Boot lock disabled)
IPCCDBA : 0x3FFF (0x3FFF)
Security Configuration Option bytes ESE:
ESE : 0x0 (Security disabled)
PCROP Protection:
PCROP1A_STRT : 0xFF (0x803FC00)
PCROP1A_END : 0x0 (0x8000000)
PCROP_RDP : 0x1 (PCROP zone is erased when RDP is decreased)
PCROP1B_STRT : 0xFF (0x803FC00)
PCROP1B_END : 0x0 (0x8000000)
Write Protection:
WRP1A_STRT : 0x0 (0x8000000)
WRP1A_END : 0x1 (0x8000800)
WRP1B_STRT : 0x7F (0x803F800)
WRP1B_END : 0x0 (0x8000000)
OPTION BYTES BANK: 1
Q.: I cannot start my own program at 0x8000000
How can I remove write protection? or possibly to another Addr. move
Q.: Is there a chance to start my own program on this board?
Solved! Go to Solution.
‎2021-08-29 11:33 AM
You should be able to change WRP1A_STRT/WRP1A_END in STM32CubeProgrammer somewhere within the option bytes.
‎2021-08-29 4:45 AM
Attach picture or Web link to specific board you're talking about.
​
STM32 Cube Programmer should permit you to remove of change settings.
​
You could probably also put code deeper into flash, using the existing boot loader if you understood it's specific requirements and expectations. Download the binary data in there currently and attach.​
‎2021-08-29 5:03 AM
‎2021-08-29 11:33 AM
You should be able to change WRP1A_STRT/WRP1A_END in STM32CubeProgrammer somewhere within the option bytes.
‎2021-08-29 10:41 PM
@TDK, thx that works for me.:grinning_face: