2025-01-08 06:28 AM
I have two custom STM32WB55 boards that I initially started with the P2P_Client/Server projects. I have the two devices communicating with each other. Once the communication is established, the notification characteristic is enabled from the P2P_Client, and data starts flowing from the server to the client. Next step is to try and disable/enable the notification programmatically from the P2P_Client. I see in the p2p_client_app.c file, there is an event handler for, APP_BLE_ENABLE_NOTIFICATION_DESC and APP_BLE_DISABLE_NOTIFICATION_DESC.
Can anyone point me to the correct process for either setting the status somehow so that the event handler is utilized or what is the recommended process for enabling/disabling a notification programmatically from the P2P_Client?
Kindest regards.
Solved! Go to Solution.
2025-01-31 02:46 AM
Hello @kumaichi
To Enable/Disable notifications, you can use the aci_gatt_write_char_desc function on the context of update_Service() in p2p_Client_app.c. This will set the Client Characteristic Configuration Descriptor (CCCD) of the "Notify" Service to enabled or disabled.
For more details, you can have a look at the p2p_Client_app.c file of the ST Client node example.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-31 02:46 AM
Hello @kumaichi
To Enable/Disable notifications, you can use the aci_gatt_write_char_desc function on the context of update_Service() in p2p_Client_app.c. This will set the Client Characteristic Configuration Descriptor (CCCD) of the "Notify" Service to enabled or disabled.
For more details, you can have a look at the p2p_Client_app.c file of the ST Client node example.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.