cancel
Showing results for 
Search instead for 
Did you mean: 

Powering a peripheral using STM32WB5MM-DK

Hichamm
Associate II

This might be a dumb question but can the STM32WB5MM-DK power a 3.3V peripheral device?
This part of the user manual makes it sound like the whole Arduino shield should not be used to supply any sort of power:

Hichamm_0-1725405128898.png

Yet according to this table, pin 4 should be able to do what I need 

Hichamm_1-1725405271500.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @Hichamm 

"Do not supply 3.3 V or 5 V from the ARDUINO® shield. Supplying 3.3 V or 5 V from the
ARDUINO® shield could damage the STM32WB5MM-DK Discovery kit" means that you should not supply the STM32WB5MM-DK board with the ARDUINO connector. But you can use the 3V3 pin or the 5V to supply your sensors for example.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @Hichamm 

"Do not supply 3.3 V or 5 V from the ARDUINO® shield. Supplying 3.3 V or 5 V from the
ARDUINO® shield could damage the STM32WB5MM-DK Discovery kit" means that you should not supply the STM32WB5MM-DK board with the ARDUINO connector. But you can use the 3V3 pin or the 5V to supply your sensors for example.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hichamm
Associate II

Thanks, the wording made it quite misleading but it makes sense now.