cancel
Showing results for 
Search instead for 
Did you mean: 

P-Nucleo-WB55 Low power examples

MahmoudAhmed11
Associate III

Hello
I was developing an application that uses BLE and low power mode. I was testing that on a custom board and when I measured the current consumption at STOP2_MODE, it was 1.7 mA.
I expected that I had made a mistake. So I tried the low power examples found there STM32CubeWB/Projects/P-NUCLEO-WB55.Nucleo/Examples/PWR at master · STMicroelectronics/STM32CubeWB on my board and then using the P-Nucleo-WB55 and I found the current consumption is above 4 mA.
Shouldn't be measured in micro-ampere? I am confused now, as I am using an ST example and a dev board, so it should work well.

Thanks in advance.

 

Best regards,

Mahmoud A.

1 ACCEPTED SOLUTION

Accepted Solutions
FilipKremen
ST Employee

Hello,

before measurement with NucleoWB55 please remove everything from JP5 and JP2, also remove USB cable from ST-Link during measurement.

Please let me know if you can reach the stop mode current, thanks.

Best regards,

Filip Kremen

 

View solution in original post

3 REPLIES 3
MahmoudAhmed11
Associate III

?

FilipKremen
ST Employee

Hello,

before measurement with NucleoWB55 please remove everything from JP5 and JP2, also remove USB cable from ST-Link during measurement.

Please let me know if you can reach the stop mode current, thanks.

Best regards,

Filip Kremen

 

Hello @FilipKremen,
Yes, it solved the problem. 
Thanks for your help.