2025-06-09 5:56 AM
Hello,
I updated my development kit with the example IOT_HTTP_WebServer from the example selector in STM32 IDE. Then I needed to upgrade the firmware on wifi module, which seemed to work. I think I can connect to wifi, but I cannot open a webpage when I paste the IP address, with all demonstrations for pressure, humidity, etc. The web page is searching and in the end I get a message the page cannot be found.
What can this depend on? Yhe following is what I get on the Tera terminal when I sign in the network:
Selected Access Point INS-GUEST ch 6 rss -48 Security WPA2-AES country .CN bssid 0a.8d.db.db.4c.2c
C:/Users/xxxxxx my name here/STM32CubeIDE/workspace_1.18.1/IOT_HTTP_WebServer/WebServer/Target/net_interface.c:191 main ... 0x2000004c 0x20000c6c "xxx WIFI-NETWORK name here "
- Network Interface starting:
- Network Interface ready:
- Device Name : MXCHIP-WIFI.
- Device ID : EMW3080B.
- Device Version : V2.3.4.
- MAC address: 84.9d.c2.96.d7.b9
- Network Interface connecting:
- Network Interface connected:
- IP address : 192.168.1.213.
*** Create TCP socket
*** TCP socket created
*** net_setsockopt ...
*** Set port and bind socket
*** Port and socket binded
*** Listen for incoming connections
*** Listening started
--> Please connect to 192.168.1.213:80
2025-06-09 8:39 PM
Hello @GTanova ,
Ensure no firewall or network restrictions block communication.
You can test the board with another example (e.g., IOT_MQTT_Client) to verify network functionality.