On STM32 cube I-CUBE-LRWAN, GPIOS sx1276
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-01-22 6:33 AM
#define RADIO_TCXO_VCC_CLK_ENABLE() __HAL_RCC_GPIOA_CLK_ENABLE()
#define RADIO_ANT_SWITCH_CLK_ENABLE_RX() __HAL_RCC_GPIOA_CLK_ENABLE()
#define RADIO_ANT_SWITCH_CLK_ENABLE_TX_BOOST() __HAL_RCC_GPIOC_CLK_ENABLE()
#define RADIO_ANT_SWITCH_CLK_ENABLE_TX_RFO() __HAL_RCC_GPIOC_CLK_ENABLE()
FIRST: TXCO ENABLE/DISABLE, RIGHT ?
SECOND: TRANSMIT/RECEIVE ANTENNA DIRECTION
THIRD: ?
FOURTH: ?
Thank you!
- Labels:
-
LoRa
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-01-28 2:25 AM
hello @MWisi.1​ ,
FIRST: TXCO ENABLE/DISABLE => Yes
SECOND: TRANSMIT/RECEIVE ANTENNA DIRECTION => RECEIVE ANTENNA DIRECTION
THIRD: TX BOOST => LP mode up to +15dBm and HP mode up to +22dBm
FOURTH: TX : => TRANSMIT ANTENNA DIRECTION
BR,
Bruno
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-01-28 4:23 AM
Hi @Bruno_ST​
SECOND: TRANSMIT/RECEIVE ANTENNA DIRECTION => RECEIVE ANTENNA DIRECTION
FOURTH: TX : => TRANSMIT ANTENNA DIRECTION
wow, looks that uses two GPIOS, one to enable receive (HIGH), and one to enable transmit (HIGH)
My module use only one GPIO to enable transmit (HIGH) and enable receive (LOW).
Maybe i will have to modify the STM32 CUBE LRWAN code, right ?
Because my examples in
My LoRaWAN Semtech project (KEIL) and my LoRaWAN LMIC project (Arduino), uses the
#define RADIO_ANT_SWITCH_HF PA_15 (keil)
.rxtx = RADIO_ANT_SWITCH_HF, (lmic)
Use 1 GPIO to control the direction.
And i right ?
Tks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-01-28 5:15 AM
second: in order not to get in troubles:
There is some error that occurs because of the length of pathnames -on windows- you can copy and paste the project to shorten the path name and then I was able to program the module to use it as AT command slave.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-01-28 5:39 AM
Good ! So problem solved ?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-01-28 7:49 AM
Hi @ssipa.1​ and @Bruno_ST​
no, i have to modify the STM32 CUBE LRWAN because use TWO GPIOS to control the direction, transmit and receive data, am i right ?
I have to modify it to make this direction control, using only on GPIO, right ?
If confirm, i can continue! Thanks
Miguel
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-01-28 8:38 AM
@MWisi.1​
I don't know the module you are using but with I-CUBE-LRWAN and setup SX1276MB1MAS, yes there is only one pin to control TX/RX:
File sx1276mb1mas.c:
void SX1276MB1MAS_RADIO_SetAntSw(RfSw_TypeDef state)
{
switch (state)
{
case RFSW_OFF:
{
HAL_GPIO_WritePin(RADIO_ANT_SWITCH_PORT, RADIO_ANT_SWITCH_PIN, GPIO_PIN_RESET);
break;
}
case RFSW_RX:
{
HAL_GPIO_WritePin(RADIO_ANT_SWITCH_PORT, RADIO_ANT_SWITCH_PIN, GPIO_PIN_RESET);
break;
}
case RFSW_RFO_LP:
{
HAL_GPIO_WritePin(RADIO_ANT_SWITCH_PORT, RADIO_ANT_SWITCH_PIN, GPIO_PIN_SET);
break;
etc...
RFSW_RFO_LP is RFOutput so TX.
BR,
Bruno
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-01-28 9:33 AM
Expect that you'll need to review and modify the software stack to address the specifics of your implementation, and how the RF signals are gated via the RF switch/mux in-front of the antenna, and how many "ways" that can go, the number of pins involved, and the HIGH/LOW states with respect to the mode/mixing you want to occur. Perhaps start by looking at the Data Sheet for the RF part first, and how it's wired in your implementation.
Think of this from a HW perspective, not a SW Engineering one.
The Murata module implementation has THREE paths, Receive, Output Highest Power, Output Normal Power, other designs/implementations have a Receive OR Transmit, but the MUX can gate both channels on together, which you don't want
no, i have to modify the STM32 CUBE LRWAN because use TWO GPIOS to control the direction, transmit and receive data, am i right ?
I have to modify it to make this direction control, using only on GPIO, right ?
No, probably not right, look at the schematics/block diagrams. Pretty sure there's THREE on the B-L072Z-LRWAN1 (DISCO), but you're being super vague about YOUR design.
Which board are you using? Something of your own creation? The Semtech Shields?
If YOUR design has one or two pins you'll need to walk the software and do a clean port for your implementation that fully takes into account the modes of operation, and transitions, and timing/sequencing properly. Not simply an affirmation by third-parties that it's "right" or completely handled.
Up vote any posts that you find helpful, it shows what's working..