cancel
Showing results for 
Search instead for 
Did you mean: 

No RX timeout IRQ after RX in single mode with timeout

HugoL
Associate II

If I call SUBGRF_SetRx() with a timeout of, let's say 100 ticks in LoRa mode, I don't get an RX timeout IRQ at the end of the timeout.

I have checked the radio status with SUBGRF_GetStatus(). The radio goes to RX then back to standby.

I have cross-checked that SUBGRF_SetDioIrqParams() is called so RX timeout IRQ is enabled.

I have cross-checked that SUBGHZ_Radio_IRQHandler is enabled (indeed it is called after a TX).

In the datasheet the RX/TX timeout IRQ is indicated as valid for GFSK and LORA mode.

I realize that the drivers manage the radio timeouts in LoRa mode with timers, not with the radio abilities. So what I am trying to do is not covered by the examples.

Do I miss something?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ngodoanvan
Senior

Hi,

I have same problem.

Have you solved this problem yet?

If you solved this problem, please tell me how to fix this problem.

Thanks