2024-12-18 1:05 PM - edited 2024-12-18 1:12 PM
I'm trying to use STM32WB09KE for the BLE application.
However, unlike STM32WB55, this microcontroller must activate PKA and RNG for the BLE module.
So, I did.
However, after generating the BLE code, I tried to build the project in the IDE and it showed a lot of errors related to RNG part.
For example, these functions are not found in the project.
HW_RNG_Init()
blue_unit_conversion()
PKAMGR_Init()
aci_gatt_srv_profile_init()
NVMDB_Tick()
NVMDB_AppendRecord()
NVMDB_ReadCurrentRecord()
NVMDB_CompareCurrentRecord()
NVMDB_DeleteRecord()
Osal_MemCpy()
GetPartInfo()
HW_AES_Encrypt()
HW_RNG_GetRandom16()
HW_RNG_GetRandom32()
RADIO_GetMaxPALevel()
RADIO_GetDefaultPALevel()
RADIO_SetHighPower()
Do you have any idea why my IDE cannot import some files related to this?
My cubeMX and cubeIDE are latest version.
Solved! Go to Solution.
2024-12-18 1:59 PM
This problem is solved by unchecking "Generate Under Root" in the CubeMX - Project Manager - Project tap.
2024-12-18 1:59 PM
This problem is solved by unchecking "Generate Under Root" in the CubeMX - Project Manager - Project tap.