cancel
Showing results for 
Search instead for 
Did you mean: 

Missing Parameter when Configuring LCO on STM32WB05TZ FW Pack V1.0.0

DCMilla
Associate II

When configuring the LCO output on an STM32WB05TZ with STM32CubeIDE 1.16.0 using STM32Cube FW_WB0 V1.0.0, the Generated code is missing the GPIO "Alternate" parameter, as a consequence, the output does not appear in the pin.

Below is the fix that worked for me.

/*Configure GPIO pin : PB12 */ GPIO_InitStruct.Pin = GPIO_PIN_12; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF1_LCO; // <----- Missing HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 
Cheers,
David C.

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @DCMilla 

This behavior has been solved on the last version of the STM32CubeMX V6.13.0.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @DCMilla 

Thank you so much for repoorting this issue 

I confirm this issue on my side. I've escalated to the concerned team for correction on the coming releases (under internal ticket number 190763).

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

STTwo-32
ST Employee

Hello @DCMilla 

This behavior has been solved on the last version of the STM32CubeMX V6.13.0.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.