2024-05-31 1:53 AM
Some odd behavior I experience with STM32WB peripheral.
Bonding list was cleared, after having been boned with a master.
Now when same master connects to me, I get a connection and an immediate disconnection!
What may be the cause? How to prevent that behavior when clearing Bonding list on my side?
2024-06-05 1:27 AM
Hello @DS.4
the behavior you're experiencing with the STM32WB peripheral where the bonding list is cleared and then the same master connects and immediately disconnects could be related to the bonding information not being properly stored or retained after certain events, such as a reset or a forced disconnection.
To prevent the loss of bonding information and the subsequent immediate disconnection when the same master attempts to reconnect, you should:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-05 11:56 AM
Bonding list is not retained on peripheral, I actually forcefully cleared it, so its empty.
It exists only on client side ( that previously connected and bonded to that peripheral ) .
Wondering what is the flow of events on this scenario, when that client connects again?
Client knows the peripheral, but peripheral no longer knows that client.
2024-06-27 10:54 AM
Hello @DS.4
Could you please clarify more about this.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-27 10:33 PM
Interested to know what happens in this case on ;peripheral side:
1.Peripheral (STM32WB55) and client Connected -Paired - Bonded.
2. Disconnected.
3. Peripheral (STM32WB55) lost keys.( erased them e.g.)
4. Client attempts to connect ( client still has his key)
How will pairing behave on Peripheral Side? Will it disconnect the client? Will it try to repair? Is there some api commands app can use to configure/handle this scenario?