cancel
Showing results for 
Search instead for 
Did you mean: 

LoRaWAN End Node Dual Core - Can't Update Flash Map in Linker File for CM0+ Core

dbdev
Associate

MCU: STM32WL55JC1

FW Version: STM32Cube_FW_WL_V1.3.1

Reference: LoRaWAN_End_Node_DualCore

Compiler/Debugger: STM32CubeIDE

Issue:

I am trying to expand the flash memory region for the CM4 application by reducing the flash memory region of the CM0+ application. When trying to modify `STM32CubeIDE/CM0PLUS/STM32WL55JCIX_FLASH.ld`: 

From:

FLASH   (rx)   : ORIGIN = 0x08020000, LENGTH = 120K

To:

FLASH   (rx)   : ORIGIN = 0x0802A000, LENGTH = 80K

The CM0+ core will never synchronize and the applications on both cores are unable to proceed. The CM4 core boots fine, but hangs waiting for the CM0+ core. If I only reduce the LENGTH of the CM0+ core it proceeds without issue.

I have also tried to modify `Common/System/system_stm32wlxx.c` by defining USER_VECT_TAB_ADDRESS and adjusting the VECT_TAB_OFFSET with no success.

What is the correct way to modify the flash allocations?

2 REPLIES 2
STTwo-32
ST Employee

Hello @dbdev 

Could you please give more details about the changes you maid to have this issue.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

bmckenney
Senior

CPU2 boots according to the setting of SBRV (along with C2OPT) in FLASH->SRRVR [Ref RM0453 rev 3: Sec 2.3 and 4.10.20]. Out of the box, SBRV=0x8000 (and C2OPT=1), so it will boot from 0x08020000, which won't have the reset vector after you change the ORIGIN.

If you're not running in Secure mode (and you haven't changed C2BOOT_LOCK=0) I expect you can just write a different value into SRRVR:SBRV and then boot CPU2. [I haven't tried it.]