cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with LoRaWAN_FUOTA_DualCore application for Nucleo-WL55JC1

Hi there, i hope youre doing great!

 

Im exploring FUOTA over LoRa/LoRaWAN using STM32CubeWL and the Nucleo-WL55JC1

For this purpose im exploring the application (included in STM32CubeWL) "LoRaWAN_FUOTA_DualCore"

I read the 'readme' file to accomplish build and flashing of the board with this application but the build.bat file throws an error

So i decided to compile every project of the full application inside STM32CubeIDE, but in the project 'LoRaWAN_End_Node_DualCore_CM0PLUS' i found a linker error:

... LoRaWAN_End_Node_DualCore_CM0PLUS.elf section `.data' will not fit in region `APPLI_ROM'

...region `APPLI_ROM' overflowed by 272 bytes

Im using STM32CubeIDE v2.0.0 and STM32CubeWL v1.4.0, running on windows 11

Am i doing something wrong?

 

Any suggestions?

1 REPLY 1
KDJEM.1
ST Employee

Hello @GonzalezSeniorProgrammer and welcome to the Community;

 

I reported this issue internally.

Internal ticket number: 226209 (This is an internal tracking number and is not accessible or usable by customers).

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.