cancel
Showing results for 
Search instead for 
Did you mean: 

Is periodic advertising sync supported by the coprocessor?

ADing.1
Associate II

I'm trying to enable periodic sync so that another BLE device can sync with the stm32wb5mmg and receive advertising data from it. Through bluetooth sniffer I can see that the 'Sync Info' flag in the Extended Header Flags is set to zero, meaning no sync info is present.

Looking at other ble stacks, there seems to be some additional hci commands required (such as "hci le set periodic advertising"), but there doesn't seem to be any commands similar to this in the stack for the STM32WB55 coprocessor.

Is this possible on the STM32WB55? If so, how can I achieve this?

Thanks

0 REPLIES 0