cancel
Showing results for 
Search instead for 
Did you mean: 

IPCCdataBuffAddr not matching pMb_RefTable (infinite loop)

petera88
Associate

I read the other forum on this back from 2021, but changing the files didn't do anything. Is there a fix in 2024 now?

 

 

if (OptionsBytesStruct.IPCCdataBufAddr != (uint32_t) pMb_RefTable) { /* * WARNING: If there is a difference between the MAPPING_TABLE placement in memory * and the address calculated according to the IPCCDBA option byte, * to avoid writing the IPCCDBA OB by mistake, the execution enters now in a while(1){} * Read below, uncomment RCC_OscInitStruct local variable and replace #if 1 by #if 0 if you are sure */ /* USER CODE BEGIN MBMUXIF_SystemInit_Prevent_OB_Programming */ #if 1 /* USER CODE END MBMUXIF_SystemInit_Prevent_OB_Programming */ Error_Handler(); #else

 

 

2 REPLIES 2
petera88
Associate

I'm actually having quite a bit of trouble starting an STM32WL55JC project, and activating SubGHz radio. The generated code doesn't work. How necessary is the MbMux framework? Is there anyway to get a minimal application going? 

None of the dual core example project seem to work.

Hello @petera88 

If you are looking for a SUBGHZ, I may suggest you take a look at the SubGHz_Phy_PingPong_DualCore example. It should help you.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.