2019-04-24 06:44 AM
2019-04-25 02:30 AM
Effectively, the STM32WB support external PA. We plan to develop reference design with STM32WB + Ext PA in the next weeks.
Best Regards.
2019-04-25 10:42 PM
2019-04-26 02:49 AM
Hi Eugene,
Yes I speak about TX-PA and RX-LNA.
Best Regards.
Marc.
2019-04-26 06:28 AM
2019-09-02 10:11 PM
Hi Marc,
We are developing Kids tracker for In-School application and have selected STM32WB part. We find its range less for such application (typical range required 1000 meters). As you have mentioned in the above post that you are also working on it.
It will be great if we can get your advice or preliminary work like recommended circuit etc. to start with.
Although we are considering sky66112-11 FEM for this.
Your advice will be highly appreciated.
Regards,
VK Verma
2019-09-02 11:18 PM
Hi Eugene,
The first Ext PA we have designed with the STM32WB55 is the SKY66118_11
Your choice is more complex because there 3 possible paths TX/RX/Bypass) ans the possibility to connect 2 antennas.
We plan also to evaluate your reference.
Best Regards.
Marc.
2019-10-16 12:29 AM
Hi Marc,
Is there any progress in reference how to connect external PA to STM32WB55.
How to set PIN PB0 (or other pin) as TX indicator.
Best Regards,
Lukas
2019-10-16 01:45 AM
Hi Lukas,
The pin PB6 is dedicated to drive the TX/RX for the ext PA.
A dedicated application note will be soon available on st.com
Best Regards.
Marc.
2023-09-19 07:48 PM
Hi Marc,
Currently, I used the same solution of STM32WB55RG+SKY66112-11 to get more power and sensitivity, so how about the configuration for the external PLNA? Any document can provide to above question?
Thanks.