2021-06-28 7:46 AM
I'm currently using I Nucleo lrwan1 shield and STM32L073 to create a Lora end node. I downloaded the latest I cube lrwan (v2.0.0) and there is no configuration to the I Nucleo lrwan1. So I can't make it work.
So, is there anyone who has the same problem or can anyone guide me to make it work.
I also posted the problem on the TTN forum and they recommended me to ask the st community about this problem
here is the link : https://www.thethingsnetwork.org/forum/t/i-cube-lrwan-problem/48864/3
2021-07-21 8:42 AM
Where are you now? Could you recap the exact HW configuration you are using ? Are you in End-node configuration or in AT_Master configuration ? I'm trying to understand you problem to help you ? Do you drive the USI modem directly thanks to the AT-cmd or by th eway of the AT_Master. Regarding the documentation , you will find some relevant info in the UM 2073 ... regards
2021-07-21 9:33 AM
The complaint as I read it is that the NUCLEO-L073RZ examples for the NUCLEO+USI combo, as furnished by ST in the LRWAN2 kits, don't work properly out-of-the-box.
That the default UART settings/plumbing are wrong for the AT interface to the USI (I-NUCLEO-LRWAN1)
2021-07-21 9:43 AM
OK, effectively we encountered some blocking points with this package. You will find here below all the needed fixes to be applied . Major fixe is regarding the fixe applied in lora_driver.c ... Regards
in lora_driver.c in line 81 --> replace 16 by 32 size --> static uint8_t PtrTempValueFromDevice[32] ; /*to get back the device address in */
in sys_app.c --> just reorganize two statements UTIL_TIMER_Init() and Modem_IO_Init() in the SystemApp_Init(void) function
*/
void SystemApp_Init(void)
{
/* USER CODE BEGIN SystemApp_Init_1 */
/* USER CODE END SystemApp_Init_1 */
/*Initialises timer and RTC*/
/*UTIL_TIMER_Init();*/
Gpio_PreInit();
/* Configure the debug mode*/
#if 1
DBG_Init();
#endif
/*Initialize the terminal */
/*UTIL_ADV_TRACE_Init();*/
Modem_IO_Init();
/*Initialises timer and RTC*/
UTIL_TIMER_Init();
/*Set verbose LEVEL*/
/*UTIL_ADV_TRACE_SetVerboseLevel(VERBOSE_LEVEL);*/
/*Initialize the temperature and Battery measurement services */
SYS_InitMeasurement();
/*Initialize the Sensors */
EnvSensors_Init();
/*Init low power manager*/
UTIL_LPM_Init();
/* Disable Stand-by mode */
UTIL_LPM_SetOffMode((1 << CFG_LPM_APPLI_Id), UTIL_LPM_DISABLE);
#if defined (LOW_POWER_DISABLE) && (LOW_POWER_DISABLE == 1)
/* Disable Stop Mode */
UTIL_LPM_SetStopMode((1 << CFG_LPM_APPLI_Id), UTIL_LPM_DISABLE);
#elif !defined (LOW_POWER_DISABLE)
#error LOW_POWER_DISABLE not defined
#endif /* LOW_POWER_DISABLE */
/* USER CODE BEGIN SystemApp_Init_2 */
/* USER CODE END SystemApp_Init_2 */
}
in sys_app.c --> remove from MasterApp_Init(void) the Modem_IO_Init()
in sys_app.c --> remove Gpio_PreInit(void) the two follwoing statements
line 310 --> /* __HAL_RCC_GPIOA_CLK_DISABLE();*/
line 312 --? /* __HAL_RCC_GPIOC_CLK_DISABLE();*/here is the trace ( Rx pin) transmitted by the modem at reset .. Then after join accepted modem return 254 for battery level and return code OK for the sending frame . On Tx we see the AT+SEND cmd
This problem will be reported on L073 and L053 and will be present in the future next package release ...
2021-07-22 2:31 AM
@Community member - correct: the NUCLEO-L073RZ examples for the NUCLEO+USI combo, as furnished by ST in the LRWAN2 kits, do not work properly out-of-the-box.
"the default UART settings/plumbing are wrong for the AT interface to the USI (I-NUCLEO-LRWAN1)"
Indeed; plus: