Hello, If I well understood you problem you do not find the right project to run on a Nucleo-L073RZ.The last expansion package published in 2021 (V2.1) on st.com provides the AT_Master project. \Projects\NUCLEO-L073RZ\Applications\LoRaWAN\LoRaWAN_...
Hello, as you can read in the previous exchanges the problem that was present in the V2.0 has been solved. Now you can upload the V2.1. All issues have been fixed (see history exchanges to understand why there was a problem) ....regards
Should seem that the network do not respond to a Join request. If you look at the initial trace the end-device does a join request , then modem return an asynchronous event "+joinaccept" and btw goes into a Sending periodic frame processing. Now in...
OK, we see that the join has been accepted... 254 is the response to the battery level request and data has been send to the 99 port.. keep me info on the TTN result