I have bare module of murata ABZ 078,091 and 093. how to access them using arduino IDE or AT command
CASE 1:
Lets say that " i want to access ABZ 093 module with AT command".(for LORA communication)
thing that are not clear to me are:
Some document state that you dont need to connect pullup resistor to Mcu nRST( because there is inbuilt 45k inbuilt resistor).
Should i leave VDD_TCXO ,TCXO_OUT, PHO-OSC_in , PHI-OSC_OUT Floating or should i short them to ground ?
If i want to use ABZ 091 or ABZ 078 module. Do these module come factory ready to work with AT command or do i need to use I-CUBE-LRWAN?
I want to use Arduino IDE to work with these modules.
Thanks.