cancel
Showing results for 
Search instead for 
Did you mean: 

I-CUBE-LRWAN Software Expansion 1.3.0 Does not work

GChis
Associate

I have loaded SE 1.3.0 out of the box (only changed app and dev ids) onto a Nucleo board, and after a few uplinks (data) the loraserver does not send a downlink confirmation, as if the fcnt is incorrect. In fact the fCnt is OK. It could be that the MIC is invalid, but the loraserver does not trace why it does not respond to the uplink.

This is a problem with 1.3.0 as if I load a previous version 1.2.x it functions correctly.

follows trace

21:50:47.8: SEND REQUEST

TX on freq 868300000 Hz at DR 0

21:50:49.5: 151s905: PHY txDone

21:50:50.6: RX on freq 868300000 Hz at DR 0

21:50:51.9: 154s251: PHY rxDone

154s253: APP> McpsConfirm STATUS: OK

154s254: #= U/L FRAME 2 =# Class A, Port 2, data size 16, pwr 6, Channel Mask 00FF 

154s256: APP> McpsInd STATUS: OK

154s256: #= D/L FRAME 1 =# RxWin 1, Port 0, data size 0, rssi -45, snr 9

21:50:57.7: SEND REQUEST

21:51:07.8: SEND REQUEST

21:51:17.7: SEND REQUEST

TX on freq 867500000 Hz at DR 0

21:51:19.6: 181s905: PHY txDone

RX on freq 867500000 Hz at DR 0

21:51:20.8: 183s133: PHY rxTimeOut

RX on freq 869525000 Hz at DR 0

184s135: PHY rxTimeOut

184s135: APP> McpsConfirm STATUS: OK

184s136: #= U/L FRAME 3 =# Class A, Port 2, data size 16, pwr 7, Channel Mask 00FF 

21:51:27.7: SEND REQUEST

21:51:37.7: SEND REQUEST

...

D/L never arrives

Any Ideas anybody ?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0