cancel
Showing results for 
Search instead for 
Did you mean: 

I am using the CubeMX example UART_Hyperterminal_IT.ioc file to generate a IAR project to connect a P-Nucleo board to a PC running Hyperterminal. Is there code to add after you generate the project as i can't seem to get it to work? Any help appreciated.

BMart.2
Associate II
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Le Corre Pierre
ST Employee

​Hello @BMart.2​ ,

Can you indicate us the version of STM32CubeMX and STM32CubeWB you are using?

In addition, this example comes with the IAR project ready to run: Projects\P-NUCLEO-WB55.Nucleo\Examples\UART\UART_HyperTerminal_IT\EWARM

Did you try it before generating the project with STM32CubeMX?

A more precise description of what you observe would help solve your problem.

BR.

Pierre.