cancel
Showing results for 
Search instead for 
Did you mean: 

I am currently doing my first steps on linux to build RIOTos and flash it to a Nucleo STM32WL55JC. If I do the same thing (hello world) with a Nucleo-L476 everything works fine, however if i try it with the Nucleo-WL55JC i receive the following message:

TFisc.1
Associate

### Flashing Target ###

Open On-Chip Debugger 0.11.0+dev-00748-ga70bab9e5 (2022-06-28-14:36)

Licensed under GNU GPL v2

For bug reports, read

hla_swd

Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD

Info : DEPRECATED target event trace-config; use TPIU events {pre,post}-{enable,disable}

/home/thomas/myRIOT/boards/common/stm32/dist/stm32wl.cfg:4: Error: can't read "_TARGETNAME": no such variable

in procedure 'script'

at file "embedded:startup.tcl", line 26

at file "/home/thomas/myRIOT/boards/common/stm32/dist/stm32wl.cfg", line 4

make: *** [/home/thomas/myRIOT/examples/hello-world-wl/../../Makefile.include:837: flash] Error 1

if i try to flash the .bin with the stlink-flash i receive the following message:

st-flash write hello-world.bin 0x8000000

st-flash 1.6.0

2022-06-28T15:42:25 WARN usb.c: Couldn't find any ST-Link/V2 devices

As far as I know the Nucleo-WL55 uses a STLink-V3 is this the cause of my problem?

How to fix this?

lsusb

responses with

Bus 003 Device 005: ID 0483:374e STMicroelectronics STLINK-V3

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
MM..1
Chief III

Compare cfg files or use Windows...