2022-01-20 9:10 AM
Any program that I generate using STM32CubeIDE for the STM32WB with BLE enabled hangs until I comment out the following line. What needs to change in the initialization sequence?
/**
* We should never end up in this case
* However, if due to any bug in the timer server this is the case, the mistake may not impact the user.
* We could just clean the interrupt flag and get out from this unexpected interrupt
*/
while(__HAL_RTC_WAKEUPTIMER_GET_FLAG(phrtc, RTC_FLAG_WUTWF) == RESET);
Solved! Go to Solution.
2022-10-11 7:13 AM
Hello,
This issue will be fixed in next STM32CubeWB release (v1.15.0) available soon.
Best Regards