2023-01-18 12:02 AM
Hi,
I would like to use OpenBootloader on my STM32WB35 but I do not find any exemple about it. There is a repository on the official STM github but it is empty :
Maybe somebody from STM can correct this :)
I already checked the STM32Wb package and there is nothing about openBootloader inside.
Thank you.
2023-01-18 02:30 AM
Hello @RJARC.1 ?
In fact, the repo is not ready yet, we just created the repo on the GitHub side but the release is not yet ready!
If you are looking for examples, you can refer to the existent ones for L5 et WL
Hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.