cancel
Showing results for 
Search instead for 
Did you mean: 

How to set up IEEE 802.15.4 MAC on the STM32WB55RG

JLee.19
Associate II

I have a question about STM32WB55RGV6.

I will list my current progress below.

- First of all, I will be using the NUCLEO-WB55RG board to use the IEEE 802.15.4 MAC Stack.

- I want to communicate with the Xbee S2C (XB24CZ7WIT-004) from Digi to send and receive data via USB UART.

- The configuration of Xbee S2C is as shown in the picture below. (PanID : 0x3332, Channel : 0x0C ...)

- The link below is the information of Digi Xbee S2C.

https://www.digi.com/resources/library/data-sheets/ds_xbee_zigbee?view=fullscreen

- The connection configuration is as shown in the "Block Diagram" photo below.

- I used the example in the link https://github.com/STMicroelectronics/STM32CubeWB

- The current version of STM32WB Copro Wireless Binaries is 1.16.0.

- The current FUS version is V1.2.0.0.

- "...\STM32CubeWB-master_Origin\STM32CubeWB-master\Projects\P-NUCLEO-WB55.Nucleo\Applications\Mac_802_15_4\Mac_802_15_4_FFD\STM32_WPAN\App:" I modified the "app_ffd_mac_802_15_4.c" file in this path to fix the Channel and Panid, but there is no communication.

Question.

1. what steps should I take to communicate with DIgi Xbee S2C in this state?

2. is the Coprocessor binary I set up the right one?

3. please let me know if there is any example of ST in the link https://community.silabs.com/s/article/connect-tutorial-1-getting-started-with-application-development?language=en_US that I can use in 3) MAC Mode.

Thank you.

best regards

Translated with DeepL

3 REPLIES 3
DineshB
Associate III

JLee i am also trying to do same thing but there is any proper application note to implement 802.15,4 MAC layer if you get some solution then please let me know.

Thanks and Regards

Dinesh Bisen

We're still looking for resources.

I'll let you know when I find something new.

I hope you'll do the same.

Yes JLee i am also looking for resources even i have generated case but still didn't received response from ST team.