2020-08-12 10:39 PM
I have followed the workshop on https://www.youtube.com/watch?v=V_qVURNbWuM&list=PLnMKNibPkDnHCD2Xc_xX-nWR7AoWBPK2Q. And the first time I went through it everything worked fine.
However, when I tried it a second time it did not:
I loaded the BLE_Ota_x.bin to the board using the programmer. I then use the ST BLE Sensor app to upload BLE_p2pServer_ota_x.bin into the board and set the memory allocation to 0xC000. This upload works well, but then if I want to load a new code through the app, e.g. the BLE_HeartRate_ota_x.bin, it does not work.
The file does not appear as selected firmware, after tapping the SELECT FILE button and selecting the file. If instead, I tap the round button with the refresh arrow, I get a message saying "No node was found".
I tried using the dongle in transparent mode as well and get an error or no response message after trying to upload the code.
Thanks in advance.
Cheers,
Derek
2020-08-13 8:41 AM
I did not check the content of the MOOC but just note that you cannot upgrade the FUS twice on a STM32WB device.
Once a version of FUS is installed on the chip, you will get error if you try to install it a second time.
This is not the case for the wireless stack.
Just check this point, avoid any new FUS installation.
2020-08-13 8:55 AM
Did you erase the previous BLE_p2pServer_ota_x.bin before loading the BLE_HeartRate_ota_x.bin?
Why using 0xC000? I use 0x7000 as start address for the OTA download. Note that it should not make a difference.
2020-08-13 7:51 PM
I do not erase the previous BLE_p2pServer_ota_x.bin before loading the BLE_HeartRate_ota_x.bin. In the app, I can't select a file with the "Application Coprocessor Binary" or the Custom option. When trying to upload code using the RF-Monitor, I get no response (See attached image). Regarding the previous comment, there might have been more than one attempt to upgrade the FUS, since I was not the only one working with the board.
2020-08-13 8:08 PM