2022-12-02 02:21 AM
HI Team,
We are using the STM32WB controller for our project, in that we are using the I2C1 for to communicate with Eeprom Module.
Can anyone explain how to configure/Calculate the Exact Timing Register value. If we have any sample calculator for different I2C Speeds along with other register settings it is very helpful to us.
Currently My Register value: hi2c1.hi2c1.Init. Timing = 0x00000E14, for which I2C speed it is calculated we are not understanding.
Regards,
Srinivas.V
2022-12-08 07:34 AM
Could you please share with me your inputs.
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-12-08 09:33 AM
Hi Khalsi,
Thanks for your reply. Here with I am sharing my inputs.
Please suggest me the correct settings.
hi2c1.Instance = I2C1;
hi2c1.Init.Timing = 0x00000E14; //100Khz //
hi2c1.Init.OwnAddress1 = I2C_ADDRESS;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
HAL_I2CEx_ConfigAnalogFilter(&hi2c1, I2C_ANALOGFILTER_ENABLE);
HAL_I2CEx_ConfigDigitalFilter(&hi2c1, 0x0)
HAL_I2CEx_EnableFastModePlus(I2C_FASTMODEPLUS_I2C1);
/*##-1- Configure the I2C clock source. The clock is derived from the SYSCLK #*/
RCC_PeriphCLKInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2C1;
RCC_PeriphCLKInitStruct.I2c1ClockSelection = RCC_I2C1CLKSOURCE_SYSCLK;
//GPIO Configuration
GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;//GPIO_SPEED_FREQ_LOW,GPIO_SPEED_FREQ_HIGH,GPIO_SPEED_FREQ_MEDIUM,GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF4_I2C1;
I have added source file also for your reference in attachments.
Please let me know if any more inputs are required from my side.
2022-12-09 12:50 AM
Hello,
The "Excel spreadsheet I2C_Timing_Configuration_V1.0.1" is only for the STM32F3 and STM32F0
(I2C timing configuration tool for STM32F3xx and STM32F0xx microcontrollers)
I recommend you to use the STM32CubeMX for getting Higher speeds like 400Khz and 1 MHz, it helps you to configure/Calculate the Exact Timing Register value.
Foued.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-12-09 01:16 AM
Hi Khalsi,
Once again thanks for your reply and support. In STM32CubeMX Some of the fields are not able to calculate like Rise & Fall times, and what is the impact of these two variables also we do not know and currently we keep it as zero's only.
If you have any other I2C example code integrated with specific application is useful to us.
Regards,
Srinivas.V
2022-12-09 01:17 AM
Hi Khalsi,
Once again thanks for your reply and support. I have shared my code files in last message, could you find out any changes are required in that, please let us know, it is very helpful to us to relook into that one.
2022-12-09 01:46 AM
Hello,
You can check the I2C examples from :
\Repository\STM32Cube_FW_WB_V1.15.0RC2\Projects\P-NUCLEO-WB55.Nucleo\Examples\I2C
Download the STM32Cube MCU Package for STM32WB series :
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-12-09 02:11 AM
Example description:
-I2C pins
-I2C Clock Source Frequency : 32 MHz
-I2C Speed Frequency : 1MHz
-Rise Time : 0 ns
-Fall Time : 0 ns
Code:
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV1;
RCC_OscInitStruct.PLL.PLLN = 8;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Configure the SYSCLKSource, HCLK, PCLK1 and PCLK2 clocks dividers
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK4|RCC_CLOCKTYPE_HCLK2
|RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.AHBCLK2Divider = RCC_SYSCLK_DIV2;
RCC_ClkInitStruct.AHBCLK4Divider = RCC_SYSCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief Peripherals Common Clock Configuration
* @retval None
*/
void PeriphCommonClock_Config(void)
{
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/** Initializes the peripherals clock
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SMPS;
PeriphClkInitStruct.SmpsClockSelection = RCC_SMPSCLKSOURCE_HSI;
PeriphClkInitStruct.SmpsDivSelection = RCC_SMPSCLKDIV_RANGE1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN Smps */
/* USER CODE END Smps */
}
/**
* @brief I2C1 Initialization Function
* @param None
* @retval None
*/
static void MX_I2C1_Init(void)
{
/* USER CODE BEGIN I2C1_Init 0 */
/* USER CODE END I2C1_Init 0 */
/* USER CODE BEGIN I2C1_Init 1 */
/* USER CODE END I2C1_Init 1 */
hi2c1.Instance = I2C1;
hi2c1.Init.Timing = 0x00100413;
hi2c1.Init.OwnAddress1 = 0;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
Error_Handler();
}
/** Configure Analogue filter
*/
if (HAL_I2CEx_ConfigAnalogFilter(&hi2c1, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
{
Error_Handler();
}
/** Configure Digital filter
*/
if (HAL_I2CEx_ConfigDigitalFilter(&hi2c1, 0) != HAL_OK)
{
Error_Handler();
}
/** I2C Enable Fast Mode Plus
*/
HAL_I2CEx_EnableFastModePlus(I2C_FASTMODEPLUS_I2C1);
/* USER CODE BEGIN I2C1_Init 2 */
/* USER CODE END I2C1_Init 2 */
}
Foued
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-12-09 03:09 AM
Hi Khalsi,
Once again thanks for your support and sharing the source code to us.
Almost code is the same except the Clock Source settings, in your code RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK.
our code,
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSE.
but the Input Clock to I2C1 is 32 MHz Only, Mx settings also same. We will use Same Timing Reg value for our as well.
Similar way can you have any code base for Flash operations initializations and Read, Write and Erase as well. We will use the same for our purpose.
Regards,
Srinivas.V