cancel
Showing results for 
Search instead for 
Did you mean: 

How do I achieve 2 Mbit/s (or close to that) data rate on STM32WB55 ?

SStoy.1
Associate II

Hi,

 

I am running the BLE_DataThroughput example for the STM32WB55 with two boards as described in the documentation- one set as a client, one as a server. I have connected the client board to a desktop PC via UART, and I am monitoring the output with PuTTy. With this setup, the highest data throughput rate I get is ~ 98 600 bytes/s as reported at the UART by the board. This is with PHY = 2M. When I press the SW2 button on the baord it switches to PHY = 1M, and the data throughput rate falls to ~2 500 bytes/s. My question is whether this is normal and how can I get the advertised 2 Mbit/s datarates for this chip, or at least something closer? The current data rate corresponds to ~ 0.8 Mbit/s.

 

I referred to AN5289 Building wireless applications withSTM32WB Series microcontrollers, section 7.6.5- How to maximize data throughput where it is advised that I set the connection interval and connection event length at 50 ms, which I did correctly as far as I can tell. The effect this produced was to increase the PHY=1M data rate from ~ 2 500 bytes/s to ~ 30 000 bytes/s, however the PHY=2M data rate was reduced from ~ 98 600 bytes/s to ~ 85 000 bytes/s. What am I doing wrong? How can I get the advertised 2 Mbit/s (or at least close to that)? These data rates are for the two boards almost on top of each other so loss due to range is not a problem.

This discussion is locked. Please start a new topic to ask your question.
9 REPLIES 9
DHunt.1
Associate II

Hi!

I have the same issue.

I used the tips from AN5289, but it didn't solve a problem. Throughput remains low for about 20 kbit/s.

If you got a result, could you please let me know what did you do?

Best Regards

Den

Hi,

No, unfortunately, I do not have an answer yet. I will post here if I find a working solution. Please do the same if you come up with one first. Meanwhile I am looking at Nordic Semiconductors' forums as it seems they offer better support and more discussion. The microcontroller they offer is quite similar. I think they use the same Bluetooth stack so my thinking is that if it is some parameter configuration that would allow fast data rate, it would work both on the STM32WB55 and the nRF.

Best,

Svet

RNiel.2
Associate II

Hi,

When I tried the example back in February I managed to get a throughput of 171 kBytes/s (close to theoretical maximum). I have since tried to recreate the performance with a custom service, though without any luck as my throughput is limited to 47 kBytes/s. So I tried to go back to the data throughput example to see what I did differently.

Going back to the data throughput example I can now reach a maximum of 153 kBytes/s with the following settings.

In app_conf.h

#define CFG_TX_PHY  2

#define CFG_RX_PHY  2

In app_ble.c -> Connection_Update(void)

I changed the CONN_P1_400 and CONN_P2_400 to CONN_P2_50 and CONN_P2_50. I know data throughput should be best at 400 ms but I got better results this way.

And most importantly I build the project with release setting instead of debug, in CubeIDE. This increased both the throughput and stability of the connection.

Does these settings help you, @DHunt.1​ and @SStoy.1​ ?

(I still haven't managed to increase throughput on my custom service above the 47 kBytes/s)

Best,

Robert

Hi,

First, thank you for replying! I have tried these configurations of

#define CFG_TX_PHY  2

#define CFG_RX_PHY  2

and changing the CONN_P1_400 and CONN_P2_400 to CONN_P2_50 and CONN_P2_50 but unfortunately, I was unable to get such a good result. I also tried building with release instead of debug settings. This refers to the little drop-down menu that pops up from the little hammer 'build' button in STM32CubeIDE, correct? Unfortunately, this did not improve throughput for me either. I am still stuck at ~96000 bytes/s.

Is it possible for you to upload the project where you manage 150-170 kBytes/s so that I can test my boards with it?

Best,

Svet

Hi,

Weird it didn't work, I'll upload my project. Hope this works for you!

Yes, I did refer to the hammer icon release build.

This is the output I receive from the dongle

0693W000008zUFFQA2.png/Robert

Hi!

Thank you for feedback.

How did you test the throughput? I adapted your example for my application and was transmitting data via notify with aci_gatt_update_char_value_ext API ( 1 packet = 243 bytes) and achieved only 20 kbytes/s (both devices are 5.0 BLE). I called this function in systick interrupts every 5ms and got BLE_STATUS_INSUFFICIENT_RESOURCES periodically. Then I decided retransmit packets while API didn't return BLE_STATUS_SUCCESS. That was I were doing. Would you please tell me what's wrong in my coding?

Best,

Den

Hi Robert,

Thanks for your persistent help. I imported your project as is and I am still getting the same throughput~ 90 kBytes/s. I am wondering whether it might have to do something with the fact that I am using 2 separate nucleo boards to run this. You mentioned a dongle. Does that mean you are using the little dongle that arrives with the nucleo board? As far as I remember these were to be used as some sort of an RF testing tool and they do not have a debugger so you have to connect them to one to program them. Is that what you did?

Best,

Svet

Hi,

I don't think there is anything wrong with using 2 separate Nucleo boards, but I haven't tested that.

Soldering pins on the dongle makes it much easier to program and work with.

This is my setup:

  • 1B is the BLE server/peripheral it connects automatically to the client/dongle when powered on and SW1 turns on the blue LED and enables notifications.
  • 1A is the BLE client/dongle, it is programmed with the ST-link on 0B (I think there is a guide somewhere to better explain this setup). The 3 pins on the bottom is a UART-connection to the PC where I can read the data throughput in TeraTerm (baudrate 115200).
  • 0B is the programmer and debugger for 1A

0693W000008zbm1QAA.jpg 

Hope this helps,

/Robert

Hi Robert,

This is an interesting setup, thanks for showing it. I could not make the 2 nucleos to transmit at more than 90 kBytes/s unfortunately. For the record, I made sure to have the latest FUS and the full BLE stack flashed on them as per the instructions in the readme.txt file in the folder of the example. I do not see why I am not getting the transfer rates that you are.

I am now trying to set up a dongle to act as the receiver as you have done. May I ask how you transmit to your PC over UART from the dongle? is that what the 3 wires on the bottom you have connected to the dongle are for?

Can you also please tell me whether

#define CFG_BLE_CENTRAL

#define CFG_SERVER_ONLY

are the only parameters you change when uploading the BLE_DataThroughput example to your boards? I tried with the following:

#define CFG_BLE_CENTRAL 0

#define CFG_SERVER_ONLY 1

on one board, and then

#define CFG_BLE_CENTRAL 1

#define CFG_SERVER_ONLY 0

on the other, as instructed in the readme.txt of the example.

Best,

Svet