Skip to main content
Mihaita Ivascu
Associate III
May 21, 2025
Question

How change SubGHz_Phy_AT_Slave example for P2P LoraWAN

  • May 21, 2025
  • 5 replies
  • 470 views

Hello,

 

     I am running SubGHz_Phy_AT_Slave on STM32WL55JC1 board and I see when running AT commands menu that there are TX and RX tests. 

    I would like to use that example for peer to peer LoraWAN  between two STM32WL55JC1 boards meaning one sends 100 bytes using Radio and t he second one receives it and acknowledges but I am not sure how to modify that example.

     I have seen that there are suggestions about modifying some examples for using only Radio.Send and Radio.Recv for having peer to peer but not sure how it applied to this SubGHz_Phy_AT_Slave example.

    In that example I see that the TX and RX tests use some random generated payload(with Prbs9_generator)

    Has anyone used peer to peer Lorawan between 2 o boards successfully with the ST examples?

 

Thanks,

     Mihai

 

 

 

This topic has been closed for replies.

5 replies

Andrew Neil
Super User
May 21, 2025

@Mihaita Ivascu wrote:

peer to peer LoraWAN 


That doesn't make sense: LoRaWAN is, by definition, a "star" network - it is not peer-to-peer.

https://lora-alliance.org/about-lorawan/ 

Do you mean just LoRa - not LoRaWAN ?

For that, see the "Ping-Pong" example ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Mihaita Ivascu
Associate III
May 21, 2025

Yes, I meant Lora. Sorry

STTwo-32
ST Technical Moderator
May 21, 2025

Hello @Mihaita Ivascu 

As said TDK, for P2P communication, LoRa is what we are toking about. So, you may can use the SubGHz_Phy_PingPong and the STM32WL-SubGHz-PhyBasic-Tx-Rx. For the AT commands, you need to configure your own example based on the LoRa examples and you can refer to the LoRaWAN_AT_Slave just to know how to AT Command works.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Mihaita Ivascu
Associate III
May 21, 2025

Or I should use the PingPong example and add there the AT commands code ?

 

Thanks,

     Mihai

 

Andrew Neil
Super User
May 21, 2025

So you do just want LoRa - not LoRaWAN - then?

 


@Mihaita Ivascu wrote:

Or I should use the PingPong example and add there the AT commands code ?


If you want AT commands, then you will have to add them.

The example works without AT commands.

The example illustrates communication between two nodes using LoRa modulation - which is what you wanted? 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.