Skip to main content
Associate III
May 15, 2024
Question

FUS_STATE_ERR_UNKNOWN

  • May 15, 2024
  • 4 replies
  • 1811 views

Hi,

 

I am using the P-Nucleo-WB55x board and using the latest CubeProgrammer v2.16.0 and I tried to install stm32wb5x_Safeboot_fw.bin since the release note said we need to install this FW. I have this error.

-------------

10:41:17 : Download Stack/FUS image at address 0x80F0000 ...
10:41:17 : Memory Programming ...
10:41:17 : Opening and parsing file: stm32wb5x_Safeboot_fw.bin
10:41:17 : File : stm32wb5x_Safeboot_fw.bin
10:41:17 : Size : 7.14 KB
10:41:17 : Address : 0x080F0000
10:41:17 : Erasing memory corresponding to segment 0:
10:41:17 : Erasing internal memory sectors [240 241]
10:41:17 : Download in Progress:
10:41:18 : File download complete
10:41:18 : Time elapsed during download operation: 00:00:00.256
10:41:18 : Firmware Upgrade process started ...
10:41:18 : Application is running, Please Hold on...
10:41:30 : Reconnecting...
10:41:30 : Reconnected !
10:41:30 : Error: FUS_STATE_ERR_UNKNOWN: Unknown error ----

----------------------

The error said unknown. 

Is there a solution for this?

 

thanks,

YJ

 

This topic has been closed for replies.

4 replies

STTwo-32
ST Technical Moderator
May 15, 2024

Hello @YJ99 

Can you share the screenshot of your FUS upgrade interface on Cube Programmer. It should contain the FUS and Stack Version.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
YJ99Author
Associate III
May 15, 2024

Hi @STTwo-32 

 

Now I heard that I should not install the safeboot_fw.bin since my version is good. However, I still have an issue on the CubeProgrammer. It is about the "not STM32 target found." 

this is the log. What i did is that I liked to use the Mac_802_15_4_LPM_Periodic_Transmit application while I do 802_15_4 sniffing. The sniffer is working on the other board P-Nucleo and I liked to run this periodic transmit in another P-Nucleo. I did install fw and using IDE i did compile and load by the tool, then no target found error messages showing once i did "run" click. So I connected to Cubeprogrammer and I encounter the error of no STM32 target found. Same as IDE message. How to solve this kind of issue? What makes me avoid this issue?

 

thannks,

YJ

---------

13:34:56 : STM32CubeProgrammer API v2.16.0 | Windows-64Bits
13:34:59 : UR connection mode is defined with the HWrst reset mode
13:34:59 : ST-LINK SN : 0674FF3332584B3043155032
13:34:59 : ST-LINK FW : V2J45M30
13:34:59 : Board : NUCLEO-WB55RG
13:34:59 : Voltage : 3.25V
13:34:59 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
13:35:08 : UR connection mode is defined with the HWrst reset mode
13:35:08 : ST-LINK SN : 0674FF3332584B3043155032
13:35:08 : ST-LINK FW : V2J45M30
13:35:08 : Board : NUCLEO-WB55RG
13:35:08 : Voltage : 3.25V
13:35:08 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
13:35:34 : UR connection mode is defined with the HWrst reset mode
13:35:34 : ST-LINK SN : 0674FF3332584B3043155032
13:35:34 : ST-LINK FW : V2J45M30
13:35:34 : Board : NUCLEO-WB55RG
13:35:34 : Voltage : 3.25V
13:35:34 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication

---------------------

 

STTwo-32
ST Technical Moderator
May 31, 2024

Hello @YJ99 

Could you please check that JP1 is on the right position (on the USB_STL) and try using different connection mode. Well connected, open your FUS and share the screenshot of the view (after starting FUS and read FUS).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MM..1
Super User
May 15, 2024

Im not expert for WB, but from name safeboot maybe this require some right steps to use this fw. Seems is designed maybe for this result = no access.

And WB55 nucleo is old board , for first FUS i preffer older version for example Cubeprogrammer 2.10