2020-07-15 1:38 AM
I am trying the zigbee apps in 'STM32Cube_FW_WB_V1.7.0'. However the firmware upgrade is never successful. I followed the Release Note but i can't get FUS state. I have tried with FUS 1.02 and 1.1 but it doesn't work. I thought maybe FUS is already up to date, so I tried zigbee firmware. It doesn't work, although I believe that I entered correctly the address in the binary table. I can still connect the nucleo board via stlink, but my PC no longer recognizes the USB dongle. The log is shown below, do you have any idea what is the problem?
16:26:51 : STM32CubeProgrammer API v2.4.0
16:26:55 : ST-LINK SN : 0679FF313335415043151616
16:26:55 : ST-LINK FW : V2J35M26
16:26:55 : Voltage : 3.28V
16:26:55 : SWD freq : 4000 KHz
16:26:55 : Connect mode: Normal
16:26:55 : Reset mode : Software reset
16:26:55 : Device ID : 0x495
16:26:55 : UPLOADING OPTION BYTES DATA ...
16:26:55 : Bank : 0x00
16:26:55 : Address : 0x58004020
16:26:55 : Size : 104 Bytes
16:26:55 : UPLOADING ...
16:26:55 : Size : 1024 Bytes
16:26:55 : Address : 0x8000000
16:26:55 : Read progress:
16:26:55 : Data read successfully
16:26:55 : Time elapsed during the read operation is: 00:00:00.007
16:27:38 : Old Firmware delete ...
16:27:38 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
16:27:38 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
16:27:38 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
16:27:38 : Warning: Option Bytes are unchanged, Data won't be downloaded
16:27:38 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
16:27:38 : Memory Programming ...
16:27:38 : Opening and parsing file: 0x495_FUS_Operator.bin
16:27:38 : File : 0x495_FUS_Operator.bin
16:27:38 : Size : 11584 Bytes
16:27:38 : Address : 0x08000000
16:27:38 : Erasing memory corresponding to segment 0:
16:27:38 : Erasing internal memory sectors [0 2]
16:27:39 : Download in Progress:
16:27:39 : File download complete
16:27:39 : Time elapsed during download operation: 00:00:00.609
16:27:39 : Application is running
16:27:47 : Reconnecting...
16:27:47 : Reconnected !
16:27:48 : Firmware delete Success
16:27:48 : Download Stack/FUS image at address 0x80a9000 ...
16:27:48 : Memory Programming ...
16:27:48 : Opening and parsing file: stm32wb5x_Zigbee_FFD_Full_fw.bin
16:27:48 : File : stm32wb5x_Zigbee_FFD_Full_fw.bin
16:27:48 : Size : 306144 Bytes
16:27:48 : Address : 0x080A9000
16:27:48 : Erasing memory corresponding to segment 0:
16:27:48 : Erasing internal memory sectors [169 243]
16:27:50 : Download in Progress:
16:27:55 : File download complete
16:27:55 : Time elapsed during download operation: 00:00:06.647
16:27:55 : Verifying ...
16:27:55 : Read progress:
16:27:57 : Download verified successfully
16:27:57 : Firmware Upgrade process started ...
16:27:57 : Application is running
16:28:16 : Reconnecting...
16:28:16 : Reconnected !
16:28:16 : Error: FUS_STATE_IMG_NOT_AUTHENTIC
16:28:16 : Old Firmware delete ...
16:28:16 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
16:28:16 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
16:28:16 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
16:28:16 : Warning: Option Bytes are unchanged, Data won't be downloaded
16:28:16 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
16:28:16 : Memory Programming ...
16:28:16 : Opening and parsing file: 0x495_FUS_Operator.bin
16:28:16 : File : 0x495_FUS_Operator.bin
16:28:16 : Size : 11584 Bytes
16:28:16 : Address : 0x08000000
16:28:16 : Erasing memory corresponding to segment 0:
16:28:17 : Erasing internal memory sectors [0 2]
16:28:17 : failed to erase memory
16:28:17 : failed to erase memory
16:28:17 : Failed to download FUS operator!
16:28:17 : Retry -- 0
16:28:17 : Old Firmware delete ...
16:28:17 : Warning: Option Byte: nSWboot0, value: 0x0, was not modified.
16:28:17 : Warning: Option Byte: nboot0, value: 0x1, was not modified.
16:28:17 : Warning: Option Byte: nboot1, value: 0x1, was not modified.
16:28:17 : Warning: Option Bytes are unchanged, Data won't be downloaded
16:28:17 : Succeeded to set nSWboot0=0 nboot1=1 nboot0=1
16:28:17 : Memory Programming ...
16:28:17 : Opening and parsing file: 0x495_FUS_Operator.bin
16:28:17 : File : 0x495_FUS_Operator.bin
16:28:17 : Size : 11584 Bytes
16:28:17 : Address : 0x08000000
16:28:17 : Erasing memory corresponding to segment 0:
16:28:17 : Erasing internal memory sectors [0 2]
16:28:17 : Download in Progress:
16:28:17 : File download complete
16:28:17 : Time elapsed during download operation: 00:00:00.557
16:28:17 : Application is running
16:28:25 : Reconnecting...
16:28:25 : Reconnected !
2020-07-30 7:03 AM
There are many separate issues there.
When using the SWD interface, be sure to set the nSWboot0 to 1 before switching the USB interface in DFU mode.
Then set the reset mode to hardware mode.
Note that is not possible to read the FUS version via the SWD port. This isthe reason why this feature in not available with the GUI interface.
the FUS_STATE_IMG_NOT_AUTHENTIC error message may result from a previous FW installation. Be sure to perform a partial mass erase of the user part of the flash memory to ensure a clean memory before any programming.
Ler me know if all these remarks were helpful.