cancel
Showing results for 
Search instead for 
Did you mean: 

Error in STM32WL5MOC User Manual (UM3127, rev 3, Jan 2025)

jcwren
Associate

There is an error in table 17 on page 33 in regards to two of the pin positions for the MB1880A adapter.  Table 17 states that pin 2 is SPI1_MOSIP (PA7) / UART1_TX (PC1) and pin 3 is SPI1_MISOP (PA6) / UART1_RX (PC0).  These two pins are reversed in both the CN2 and CN3 columns.

In actuality, pin 2 is SPI1_MOSIP (PA7) / UART1_RX (PC0) and pin 3 is SPI1_MISOP (PA6) / UART1_TX (PC1)

This is confirmed by table 13 (page 28), the MB1779 schematic (MB1779-HIGH-BAND-B02 Board schematic under the B-WL5M-SUBG1 CAD Resources tab), and wasting an hour trying to determine why the I2C3 port was not talking to a device.

1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello All,

This issue is fixed in the latest release UM3127 Rev4.

Thank you for your contribution.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

3 REPLIES 3
Issamos
Lead II

Hello @jcwren 

It is a typo on the doc. @Imen.D could you please report this typo and move the post to the wireless forum since it is related to a wireless product.

Best Regards.

II

Imen.D
ST Employee

Hello @jcwren , @Issamos 

Thank you for bringing this to our attention.

An internal ticket number 219127 is submitted in order to fix this error in the coming releases of UM3127.

(PS: Ticket number 219127 is an internal tracking number and is not accessible or usable by customers).

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Imen.D
ST Employee

Hello All,

This issue is fixed in the latest release UM3127 Rev4.

Thank you for your contribution.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen