cancel
Showing results for 
Search instead for 
Did you mean: 

Digital signal input

Lep
Senior

The sampling frequency is 256kHz, it is an ADC that collects ECG signals.(The question is really not about ADC), what should I belong to with this question?

My problem is that the analog signal is output in four channels in parallel after the ADC, when clk2 is rising edge (256kHZ), the digital signal of 4bit is output (D3 D2 D1 D0). I want to use stm32wb55rgv6 to capture these signals, where should I start?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
MM..1
Chief III

You can edit your primary message and not create dupl