cancel
Showing results for 
Search instead for 
Did you mean: 

Custom Applications on STM32WB55 Coprocessor

Richard1
Associate

Hello everyone,

I wonder if it is possible to develop and run a custom coprocessor firmware on the Cortex-M0 of the chip. From what I understood so far, the FLASH and RAM portions dedicated to FUS, Safeboot, and Wireless Stack are locked from the factory, with the FUS being the only possibility to write anything to it. And since the FUS appears to perform a digital signature check for any firmware sent to it, there isn't an easy way to flash your own. So, is there an official way to do it?

From what I understand about the boot process of CPU2 (i.e., the Cortex-M0), it gets started by the CPU1, but its start offset from the secured option bytes. The manuals (and my own unsuccessful attempt) tell me that the secured option bytes can only be written by the CPU2, so any normal attempt to write to them (e.g., with the STM32CubeProg tool) will fail. But shouldn't I be able to, in principle, create a program for the Cortex-M0, write it so some designated portion of the flash, disable all the security and write the appropriate offsets to the option bytes (e.g., SFSA, SBRV, ...) and then kick off the CPU2 from within my CPU1 application? Or at least use the FUS to flash an image that I created myself? Is there any documentation on this?

Kind Regards,

Richard

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Remy ISSALYS
ST Employee

Hello,

Unfortunately, the code expected to be executed by the CPU2 must be encrypted with specific ST key that the FUS (Firmware Update Service) is the only one to manage.

Best Regards

TwisteR
Associate II

Hello,

I've asked the same question a couple of days ago. And, as expected, had been given a similar answer. I don't get it, why keep talking about how FUS works whereas people are asking on how to wipeout FUS completely and use Cortex-M0 for regular tasks (even if there will be no radio support).

There is still a glimpse of hope (see last messages), although I'm not very optimistic about it.

Remy ISSALYS
ST Employee

Hello,

It's not possible to wipeout the FUS completely and use Cortex-M0 for regular tasks.

Best Regards