2019-06-23 4:12 AM
Hello everyone,
I'm trying to build a server application with the STM32WB55 but I can't get the advertising state. I took example on the server example in the STM32Cube_FW_WB_V1.0.0 and I think it is pretty similar but it doen't work as intended.
I made some researches and I find someone with the same problem here : https://community.st.com/s/question/0D50X0000AhPJcCSQW/trying-to-get-the-advertising-state . However the proposed solution didn't work for me and I still can't get the advertising state. The programm doesn't run APPE_SysUserEvtRx() because I don't receive VS_HCI_C2_Ready I think.
Would anyone has any idea on why it behaves this way and how to solve this problem ?
Thank you.
2019-11-28 2:54 AM
Hello all,
If some of you encounter problems to detect the Stack ready event (like I), please find my code below (working fine).
Note that this event is named SHCI_SUB_EVT_CODE_READY in shci.h, not VS_HCI_C2_Ready, as mentioned earlier in this thread.
void APPE_SysUserEvtRx (void * pv_iPayload)
{
tSHCI_UserEvtRxParam * pst_userEventRxParam = NULL;
TL_AsynchEvt_t st_asynchEvt = {0};
/* Get SHCI evt code from payload */
pst_userEventRxParam = (tSHCI_UserEvtRxParam*)pv_iPayload;
memcpy(&st_asynchEvt, pst_userEventRxParam->pckt->evtserial.evt.payload, sizeof(st_asynchEvt));
/* SHCI_SUB_EVT_CODE_READY => BLE stack is ready on M0+ MCU */
if ((SHCI_EVTCODE == pst_userEventRxParam->pckt->evtserial.evt.evtcode) &&
(SHCI_SUB_EVT_CODE_READY == st_asynchEvt.subevtcode))
{
/* Your code here */
}
else {/*Nothing */}
}Enyoy.
Camille
2020-09-16 2:51 AM
Hi Camille,
Where did you find this solution? is in any official ST document?
Regards
�?lvaro
2020-09-22 9:59 AM
Hello,
Examples can be found in both Ble_Ota and BLE_RfWithFlash projects.
Regards.
2021-03-18 3:37 AM
Hello,
I've the same problem.
All buffers (like, EvtPool, SystemCmdBuffer, SystemSpareEvtBuffer,BleSpareEvtBuffer) locate in SRAM2.
But IPCC_C1_RX_IRQHandler is not called.
What did you do with it?