cancel
Showing results for 
Search instead for 
Did you mean: 

Broadcast message using B-L072Z-LRWAN1 LoRa®/Sigfox™ Discovery kit.

KK.4
Associate II

I am using B-L072Z-LRWAN1 LoRa®/Sigfox™ Discovery kit. I want to implement broadcast communication using LoRa without gateway(not LoRaWAN). As I could see from the ping pong application sample provided as part of the I-CUBE-LRWAN SDK, that nowhere node address or security key are being used. So I presume it is very much possible to broadcast it to different nodes which are actively listening using just LoRa. Request your thoughts and help on this.

2 REPLIES 2

Not sure what the question is here.

Yes, the Ping Pong example show raw methods for putting data in the air. You can layer​ node addresses or encryption to data before you send, and modify reception code to discard or further process the data.

I use these boards in a point to multipoint broadcast application.​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
KK.4
Associate II

Thanks for the quick reply.

The question was, would I be able to broadcast message from one node to multiple nodes in receiving range using LoRa(without LoRaWAN)?

Seems like it is possible. Your answer helped.