2022-05-19 1:42 PM
Not sure if this is the right place to post about CubeMX issues, but I'm having issues replicating the STM32WL55JC1 PingPong example. What I'm doing is trying to mimic every setting that exists in the example project (because it works), but some options are not actually changeable for me.
First example is here:
https://i.gyazo.com/46cebf0b8e0474d6480bd82d7e154085.png
On the right, all visibility boxes are unchecked. But in the project I'm trying to recreate the example in, I can't uncheck any of the visibility (static) boxes. It just won't let me:
https://i.gyazo.com/fdbf32a95e3c9bc8f0c5031f6c70749d.png
Second thing is in my new project, cubemx refuses to generate any bsp files. So while in the example project I have the proper BSP files:
https://i.gyazo.com/935b6558b46ce70fcf1bc5664b50d254.png
My new project doesn't have anything:
https://i.gyazo.com/8262c8d5b3e15d0a99f31d7d17be4b09.png
(Notice the lack of a BSP folder)
Both projects also match the SubGHz_Phy middleware section exactly:
https://i.gyazo.com/742ffc953bb90f3844f407dc0403bc0f.png
So the BSP files should be getting generated. They just aren't.
As a result, my new project refuses to compile. Anything I can do to remedy this? Anywhere for me to file CubeMX bugs?
Solved! Go to Solution.
2022-05-24 7:46 AM
Hello @ADrag.2 ,
Yes as you said CubeMx does not generate BSP. To add it to your project you can add to your project the file ".extSettings" that you can find in project folder's in the STM32Cube_FW_WL_V1.2.0.
In this file you will find this code :
[ProjectFiles]
HeaderPath=..\[YOUR_PATH_TO_BSP_FOLDER]\BSP\STM32WLxx_Nucleo
[Others]
[Groups]
Drivers/BSP/STM32WLxx_Nucleo=../[YOUR_PATH_TO_BSP_FOLDER]/Drivers/BSP/STM32WLxx_Nucleo/stm32wlxx_nucleo.c; ../[YOUR_PATH_TO_BSP_FOLDER]/Drivers/BSP/STM32WLxx_Nucleo/stm32wlxx_nucleo_radio.cYou just have to replace the path that match your directories to point to the Driver folder and it should work.
I will ask to know about the visibility of the functions and keep you updated.
Good luck and best regards
Louis
2022-05-19 1:57 PM
I see now that BSPs aren't generated by Cube, which is a bit deceptive since the alternative to using the bsp files are using user generated files. I still don't know where these files actually come from, but copying from the example project did the trick.
2022-05-24 7:46 AM
Hello @ADrag.2 ,
Yes as you said CubeMx does not generate BSP. To add it to your project you can add to your project the file ".extSettings" that you can find in project folder's in the STM32Cube_FW_WL_V1.2.0.
In this file you will find this code :
[ProjectFiles]
HeaderPath=..\[YOUR_PATH_TO_BSP_FOLDER]\BSP\STM32WLxx_Nucleo
[Others]
[Groups]
Drivers/BSP/STM32WLxx_Nucleo=../[YOUR_PATH_TO_BSP_FOLDER]/Drivers/BSP/STM32WLxx_Nucleo/stm32wlxx_nucleo.c; ../[YOUR_PATH_TO_BSP_FOLDER]/Drivers/BSP/STM32WLxx_Nucleo/stm32wlxx_nucleo_radio.cYou just have to replace the path that match your directories to point to the Driver folder and it should work.
I will ask to know about the visibility of the functions and keep you updated.
Good luck and best regards
Louis
2022-05-24 10:07 AM
Thank you!