2026-02-08 11:16 PM
In AN2606 Rev 69, the STM32WBA6x system bootloader section describes the UART interface as USART3, but there appear to be errors:
1. Inconsistency within the same entry:
The TX pin description mixes USART2 and USART3 in the same sentence:
USART3_TX pin Output PA12 pin: USART2 in transmission mode. Kept in reset configuration until 0x7F detected on USART_RX.
While the RX pin description correctly uses USART3:
USART3_RX pin Input PA11 pin: USART3 in reception mode. Used in alternate push-pull, pull-up mode.
2. PA11/PA12 are assigned to USART2, not USART3:
According to the STM32WBA62 datasheet, PA11 and PA12 are mapped to USART2 (USART2_RX / USART2_TX), not USART3.
Question:
Does the STM32WBA6x system bootloader actually use USART2 on PA11/PA12? It seems the document should read USART2 throughout, and the current "USART3" label is an error.
Could ST please clarify and correct this in the next revision of AN2606?
Environment:
- Document: AN2606 Rev 69
- MCU: STM32WBA62CGU6
- Section: STM32WBA6x bootloader - USART
Solved! Go to Solution.
2026-02-09 1:19 AM
Hello @bugiii.;
You are right, it is a typo in AN2606.
The supported USART interfaces for SM32WBA6 are USART1 and USART2.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-02-09 12:34 AM - edited 2026-02-09 12:47 AM
Hello @bugiii ;
Thank you for bringing this issue to our attention.
I reported it internally for checking.
Internal ticket number: 226865 (This is an internal tracking number and is not accessible or usable by customers).
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2026-02-09 1:19 AM
Hello @bugiii.;
You are right, it is a typo in AN2606.
The supported USART interfaces for SM32WBA6 are USART1 and USART2.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.