cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-TOUCHGFX 4.16.0 is out

Romain DIELEMAN
ST Employee

Hi Everyone, the TouchGFX team wishes you a happy new year.

If you haven't noticed by now, X-CUBE-TOUCHGFX 4.16.0 is out, available from CubeMX 6.0+ and from st.com as a zip (Also installable through CubeMX).

Here is the documentation for 4.16.0: https://support.touchgfx.com/

Main features:

  1. Built in support for a Gauge widget
  2. New screen transition called "Block Transition"
  3. New invalidation algorithm for improved performances

You can see all the bug fixing and improvements in the changelog.

/Romain

32 REPLIES 32
BParh.1
Senior III

How do I upgrade my existing touchgfx? Do I need to uninstall current one first?

Hi,

You do not need to uninstall the current one. You can download the latest version of TouchGFX through this official link. Just press the "Get Software" purple button.

You can also download it through STM32CubeMX. In the landing page when opening STM32CubeMX go to the "Help" tab and click on the "Manage embedded software packages". The STMicroelectronics tab will show all the available ST external tools like TouchGFX, with all available versions (TouchGFX 4.17 in my screenshot is not available to the public yet) .

0693W00000AOZn6QAH.png 

/Romain

I'm using it on a KVM Windows 10 virtual machine. I pass the STM board's USB device to the guess OS and share a filesystem containing the development resources with Samba.