cancel
Showing results for 
Search instead for 
Did you mean: 

Wondering if TouchGFX would be able to run on an STM32F411 with 512K flash & 128K of RAM. The screen I'd like to drive will take ~70K of RAM for a single display buffer.

JimFouch
Associate III

I know there is no demo that runs on a 411. I'd also have to write my own display driver to transfer the display buffer. Just wondering if the 512K Flash and remaining 58K of RAM would be enough to fit TouchGFX and my own code in.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0