Why is TouchGFX Swipe Threshold inconsistent?
I'm using the STM32F469I-DISCO board with TouchGFX. In portrait mode, I set the swipe threshold to 400 because I want the user to swipe almost all the way across the screen to switch pages. When I swipe slowly, it seems to work. However, a fast swipe changes pages with a swipe distance of only 1/2" or so. Is there a way to not make this speed-dependent? Right now, it is very easy to accidentally change pages. I want the page change to be very intentional.