2020-12-07 1:40 AM
In my code when I am using touchgfx::Unicode::UnicodeChar it is showing expected an expression....What files should I include to solve this error
Solved! Go to Solution.
2020-12-10 11:50 PM
Present documentation is actually good. What I feel is it will be helpful if you make some tutorials for adding text in other languages.
Thanks and Regards
Rishikesh G.
2020-12-10 11:54 PM
One comment to add:
TouchGFX uses 16 bit characters (UnicodeChar). Any data coming from 8-bit sources must be converted to 16bit. This can be done with Unicode::strncpy and the similar functions. These are basically just extending the (unsigned) 8-bit values to 16-bit. Then TouchGFX can show the characters, provided the font contains the characters as explained above. Typically a range of printable characters ascii are required if you plan to receive strings from say a serial port. The TouchGFXDesigner only includes the characters used by the texts in the project.
We also have a converter from UTF-8 to U16, which can be used when you received a text from eg. a cell-phone.
2020-12-11 12:42 AM
Hi RG.3,
Could you add this suggestion to the "Idea Zone" section of this forum ?
This will greatly help us keep track of this.
Best regards,
/Romain