2023-01-15 6:31 PM
Hi, I'm trying to use only one dsi data lane with OTM8009A which has two data lanes.
My MCU is STM32F769I-Eval and manuals said that this MCU has two dsi data lanes.
However, I want to use only one data lane because my custom board has only one dsi data lane.
I tried to change settings with Examples within F7Cube.
In LCD_DSI_Videomode_SingleBuffer, DSI Settings value is in there, so I change NumberOfLanes value two to one, but LCD Display doesn't work.
Is there any way to use only one data lane?
Thanks.
Solved! Go to Solution.
2023-01-15 9:57 PM
If display dont have this choice NO. Otherwise send init commands to display for setup one lane mode.
2023-01-15 9:57 PM
If display dont have this choice NO. Otherwise send init commands to display for setup one lane mode.
2023-01-15 10:23 PM
That means, If I couldn't modify the number of data lanes in display(in this case, OTM8009A), display will not work?
OTM8009A has two data lanes, and If I change the number of data lanes in STM32 to one, I think It will work strangely, but screen is only black.
When I change the number of data lanes in STM32 to two, It works properly.
2023-01-15 10:25 PM
Simply you need change on both sides of bus...
2025-02-19 12:23 AM
Hi,
I had the same problem, my MCU is STM32H747-DISCO, and LCD is MB1166-A09 drived by OTM8009A. OTM8009A datasheet said the pin LANSEL set 0 can select one data lane mode. But on MB1166 board I cannot find that pin, Is there any way to set one data lane mode?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.