2020-11-05 11:16 AM
Hello,
TouchGFX version: 4.15.0
STMCubeIDE: 1.4.2
I need some help, I am seeing some strange behavior from a custom module I am creating. Basically, when I am forced to use a PainterRGB888 to color a circle, TouchGFX will halt when calling showBaseModal()
Here is my class:
#include <gui/containers/modal/modalBase.hpp>
#include <touchgfx/Color.hpp>
modalBase* modalBase::getInstance()
{
static modalBase gModalBase;
return &gModalBase;
}
modalBase::modalBase()
{
mInternalWidth = 212;
mInternalHeight = 159;
mCornerRadius = 10;
mEdgeBuffer = 30;
mMainContainer.setX(0);
mMainContainer.setY(0);
mMainContainer.setWidth(272);
mMainContainer.setHeight(480);
circleTopLeft.setPosition(mEdgeBuffer, 161, mCornerRadius*2, mCornerRadius*2);
circleTopLeft.setCenter(mCornerRadius, mCornerRadius);
circleTopLeft.setRadius(mCornerRadius);
circleTopLeft.setLineWidth(0);
circleTopLeft.setArc(0, 360);
circleTopLeftPainter.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
circleTopLeft.setPainter(circleTopLeftPainter);
mMainContainer.add(circleTopLeft);
}
void modalBase::initialize()
{
}
void modalBase::showBaseModal()
{
if(!application().getCurrentScreen()->getRootContainer().contains(mMainContainer))
application().getCurrentScreen()->getRootContainer().add(mMainContainer);
mMainContainer.invalidate();
}
#ifndef GUI_INCLUDE_GUI_CONTAINERS_MODALBASE_HPP_
#define GUI_INCLUDE_GUI_CONTAINERS_MODALBASE_HPP_
#include <gui/common/FrontendApplication.hpp>
#include <touchgfx/containers/Container.hpp>
#include <touchgfx/widgets/Box.hpp>
#include <touchgfx/widgets/canvas/Circle.hpp>
#include <touchgfx/widgets/canvas/PainterRGB888.hpp>
#include <touchgfx/widgets/canvas/Line.hpp>
#include <gui/containers/HomeBar.hpp>
#include <touchgfx/mixins/MoveAnimator.hpp>
class modalBase
{
public:
static modalBase* getInstance();
virtual void initialize();
void showBaseModal();
protected:
FrontendApplication& application()
{
return *static_cast<FrontendApplication*>(touchgfx::Application::getInstance());
}
touchgfx::Circle circleTopLeft;
touchgfx::PainterRGB888 circleTopLeftPainter;
MoveAnimator< touchgfx::Container > mMainContainer;
private:
modalBase();//Private so no one else can make one of me.
int mInternalWidth;
int mInternalHeight;
int mCornerRadius;
int mEdgeBuffer;
};
#endif /* GUI_INCLUDE_GUI_CONTAINERS_MODALBASE_HPP_ */If I change the circle to something like a Box that doesn't require a painter, then the code works just fine. If I change it to a line (which requires a painter) then TouchGFX halts when calling showBaseModal();
If I use a circle from within TouchGFX generator, that circle will be drawn on the screen without issue.
Any idea what I am doing wrong here?
Solved! Go to Solution.
2020-11-09 10:42 PM
I believe so.
This is why I said this might be something we can optimize ^^
/Alexandre
2020-11-09 11:42 PM
The Designer will set up the canvas buffer for each view that requires it, but you can also do what you're doing to set a global buffer.